FB#.ENCLINES

Description

Used to configure the number of lines per revolution for rotary encoders. This keyword is only valid for Incremental and Sin/Cos encoders and is ignored for any other encoders and linear motors.

Context

See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Lines/revolution

Range

0 to 4,294,967,288

Default Value

1024
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
FB1.ENCLINES

3500h

02h

Unsigned32

-

-

Read/Write

No

FB2.ENCLINES

3501h

02h

Unsigned32

-

-

Read/Write

No

FB3.ENCLINES

3502h

02h

Unsigned32

-

-

Read/Write

No

FB4.ENCLINES

3503h

02h

Unsigned32

-

-

Read/Write

No

FB5.ENCLINES

3504h

02h

Unsigned32

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

FB1.ENCLINES

30080

7580

Unsigned32

Read/Write

-

FB2.ENCLINES

30081

7581

Unsigned32

Read/Write

-

FB3.ENCLINES

30082

7582

Unsigned32

Read/Write

-

FB4.ENCLINES

30083

7583

Unsigned32

Read/Write

-

FB5.ENCLINES

30084

7584

Unsigned32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.ENCLINES

30080

Unsigned32

Read/Write

-

FB2.ENCLINES

30081

Unsigned32

Read/Write

-

FB3.ENCLINES

30082

Unsigned32

Read/Write

-

FB4.ENCLINES

30083

Unsigned32

Read/Write

-

FB5.ENCLINES

30084

Unsigned32

Read/Write

-